AXIS#.VL.FB
Description
AXIS#.VL.FB returns the velocity feedback as it is received in the velocity loop after passing through Filter 3 and Filter 4.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Depends on AXIS#.UNIT.VROTARY Rotary: rpm, rps, deg/s, (custom units)/s, rad/s |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.VL.FB |
606ch |
00h |
Signed32 |
Velocity |
- |
Read only |
Yes |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6024 |
1 |
6024 (0x1788) |
AXIS1.VL.FB |
Signed32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.VL.FB |
6024 |
Float |
Read Only |
Velocity |
Related Topics